Using an MSP430F149 in the final application is showing a strange behaviour.
Measuring devices were sent back from our customers back to our service department, because they don't work anymore.
Reading code memory shows, that memory is complete empty!
Supply voltage is correct, oscillator is correct, voltage of reset is correct. If MSP430F149 is flashed once more, device works correctly again.
We have another type of device (also using this µController), which is very similar to the concerned type of device, which is not showing this behaviour.
The difference between the two types is, that the concerned device has a LCD-Display, which is controlled by MSP430F149 using SPI, and the not concerned device has an electrically isolated connection (UART) to another board, on which a different display is controlled by another processor.
Devices were sent back from different customers, so it is unlikely that a special enviroment (EMI) is responsible for this behaviour.
I found a thread here in the Forum which is also dealing with loss of memory content, but I've no idea if this is a similar problem.
Any help welcome, thank you :-).
-Bernd