I created project for grace 2.2.0.00006.
CPU: msp430g2230
I want to set up clock to 16MHz in BCS+ page, but only 1MHz precalibrated option is available.
Datasheet states, that 16 MHz is available for msp430g2230.
Is it grace bug? Any workaround?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I created project for grace 2.2.0.00006.
CPU: msp430g2230
I want to set up clock to 16MHz in BCS+ page, but only 1MHz precalibrated option is available.
Datasheet states, that 16 MHz is available for msp430g2230.
Is it grace bug? Any workaround?
EDIT: I see I was not choosing the same processor as you. The G2230 seems to have have the additional options. I will file this as a bug with the GRACE team. Int he mean time, you can use another Grace project such as for the G2553 to set up your clock as they use the same clock module. this means the code will be the same.
Hello KOSTYANTYN,
I see you are using an older version of Grace. Please update Grace tot he newest version. You can do this from within CCS by navigating to View > CCS App Center, then clicking the See More link on the top right for Code Composer Studio Add-ons. Check the Grace box for update and click the Install Software option at the top left. This should update you tot he latest version of Grace that includes the additional options such as 16MHz clock for MSP430G2553.
Regards,
JH
**Attention** This is a public forum