Hi,
I have few pins on gpio9 as key inputs.
1. does msp432 support interrupt on GPIO9
2. if Yes any sample configuration code available / ISR vector .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have few pins on gpio9 as key inputs.
1. does msp432 support interrupt on GPIO9
2. if Yes any sample configuration code available / ISR vector .
thanks Dennis for your mail.
but at the pinmux tool and a datasheet it indicates the interrupt can be configured.
this below is from the Technical reference document
this below is pinmux tool generated code
void PinMuxConfig(void)
{
//
// Configure as output pins for P9.2
//
P9DIR |= BIT2;
//
// Configure as pull-up resistor enabled pins for P9.2
//
P9REN |= BIT2;
//
// Enable interrrupt for P9.2
//
P9IE |= BIT2;
//
// Select interrrupt edge (high-to-low) for P9.2
//
P9IES |= BIT2;
}
kindly correct my understanding if I am missing some thing.
Unfortunately I don't know the pinmux tool ;\
The technical reference manual / user's guide covers a wide range of processors (in general - the MSP432P401R is the only one for now in this case). The information given in the datasheet for a specific device overrules this information or at least limits the manual in it's applicability. There may be devices having ten ports with interrupt capability later. If you have a look into the datasheet for the MSP432P401R you can see that only port 1, 2, 3, 4, 5 and 6 support interrupts. Even the first page mentions 48 I/Os with interrupt capability.
Dennis
**Attention** This is a public forum