Hi All,
I am working on a project which is based on MSP430F5438A microcontrollor. And I needs to load the firmware via UART(serially) from the PC. I have downloaded the sample project for Bootstrap Loader for MSP430F5438A. I have a few queries which are as follows
1. How to use this sample BSL project.
2. Suppose this BSL project is loaded in MSP430F5438A, how to send the firmware to Microcontroller using UART(serially). Or before sending this firmware to MSP430, we have to convert it into hex file or bin file or image file.
Thanks in advance
Regards
Jeetesh