Hi all !
I have a problem programming MSP430F2012 (not all but some uC on the same kind of board) with MSP-FET430UIF via 2-wire JTAG mode, using MSP430Flasher.
I tried both old and new firmware of the tool but I have not solved. Programming is made by pins on automatic testing bench using board power supply and connecting pins to TEST pin of uC via 1k resistor and RESET pin via 100R resistor. Reset pin is shared with reset of an ATMega64 uP assembled on the board.
The MSP430Flasher give me error "Unrecognized device Error 16" or "Fuse blown" even if uC never was secured
I use this command line: "MSPFlasher.exe" -e ERASE_ALL -v -w filename" or "MSPFlasher -m SBW2 -s -n MSP430F2012 -e ERASE_ALL -v -W Filename"
We tried other tool with this command line too: "mspfetcon +epv Filename -jtag_if=1 -FET=TIUSB" but didn't solve anyway
Anyone who had the same problem and solved ?
Thanks in advance and have a good day
Greetings, Devis