Hello,
I'm working on a Production tool built around a Raspberry Pi (ARM based processor). I'm unable to get the MSP-FET Flash Emulation Tool to work. Here's what I've done so far.
1. Downloaded latest MSP Debug Stack from http://www.ti.com/tool/mspds.
productionpi@raspberrypi:~/tiLibSources/slac460 $ mspdebug tilib --allow-fw-update MSPDebug version 0.24 - debugging tool for MSP430 MCUs Copyright (C) 2009-2016 Daniel Beer <dlbeer@gmail.com> This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. Chip info database from MSP430.dll v3.3.1.4 Copyright (C) 2013 TI, Inc. Using new (SLAC460L+) API MSP430_GetNumberOfUsbIfs MSP430_GetNameOfUsbIf Found FET: HID_FET MSP430_Initialize: HID_FET FET firmware update is required. Starting firmware update (this may take some time)... tilib: MSP430_FET_FwUpdate: MSP-FET / eZ-FET recovery failed (error = 73) tilib: device initialization failed
Two things to notice. One is obvious, I get an error message. The second is the MSP430.dll v3.3.1.4. Shouldn't this match the revision 3.8.1.0000? If I remove the libmsp430.so from /usr/lib, mspdebug will complain about not finding the file. Finally, I can use the programmer in x86 VM with no problem. I'm not sure which version of libmsp430.so I'm using.
Not really sure where to go from here?
Diego