Hi,
Have anyone of you ever tried to use Energia to program MSP430G2553 28 pin package ?
The reason I asked because the existing Engergia does not support 28 pin package. It would not recognize Port 3 pins.
What I did was using files from this site:
https //github.com/AlexJaeger/Energia/commit/07553a7689954904d56c295296b9461ac751f7d2
I created a "variant" launch pad for 28 pin package. I don't have error for unrecognize pins from Port 3. However, when I compiled it I got errors
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c: In function 'twi_init_port':
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c:218:15: error: 'TWISDA0' undeclared (first use in this function)
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c:218:15: note: each undeclared identifier is reported only once for each function it appears in
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c:218:24: error: 'TWISDA0_SET_MODE' undeclared (first use in this function)
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c:219:15: error: 'TWISCL0' undeclared (first use in this function)
G:\Energia\energia-0101E0017\hardware\msp430\cores\msp430\twi.c:219:24: error: 'TWISCL0_SET_MODE' undeclared (first use in this function)
I am not very familiar with twi.c in Energia. Can anyone shed lights on this.
Thanks for reading.