Hello,
I have an MSP430F6779A with an I2C bus activated (to drive a little oled screen).
My clocks are : MCLK = 8 MHz, SMCLK = 4 MHz and ACLK (from XT1) = 32,768 kHz.
// Set the correct VCore. core_setVcoreUp(PMMCOREV_0); core_setVcoreUp(PMMCOREV_1); core_setVcoreUp(PMMCOREV_2); // Configure XT1. UCSCTL6 &= ~(XT1OFF); UCSCTL6 |= XCAP_3; do { UCSCTL7 &= ~(XT1LFOFFG); } while (UCSCTL7 & XT1LFOFFG); // Configure DCO. UCSCTL3 |= SELREF__XT1CLK; __bis_SR_register(SCG0); UCSCTL0 = 0x0000; UCSCTL1 = DCORSEL_5; UCSCTL2 = FLLD_1 | 245; __bic_SR_register(SCG0); // Init clocks : MCLK = SMCLK = 8 MHz, ACLK = 32768 Hz. UCSCTL4 = SELA__XT1CLK | SELS__DCOCLKDIV | SELM__DCOCLKDIV;
// Divide SMCLK by 2 > 4 MHz. UCSCTL5 |= DIVS__2; __delay_cycles(250000); do { UCSCTL7 &= ~(XT1LFOFFG | DCOFFG); SFRIFG1 &= ~OFIFG; } UCSCTL6 &= ~(XT1DRIVE_3);
Here what i can see on my oscilloscope. It seems OK...
Now, i configure my I2C bus :
P2SEL0 |= BIT5 | BIT6; // Set P2.5,P2.6 to UCB0SCL, UCB0SDA UCB0CTLW0 |= UCSWRST; // Enable SW reset UCB0CTLW0 |= UCMST | UCMODE_3 | UCSYNC | UCSSEL__SMCLK; // I2C Master, SMCLK UCB0BRW_L = 10; // Divide SMCL by 10 >> 400 kHz UCB0BRW_H = 0; UCB0I2CSA = 0x3C; UCB0CTLW0 &= ~(UCSWRST); UCB0IE |= UCTXIE;
But with this code, my oled screen doesn't work because data are not correct.
If i check with my oscilloscope, i obtain 333 kHz clock with frequency divider 10, and 4 MHz / 10 is not equal to 333 kHz ???
And if i test with divider 2 (UCB0BRW_L = 2), it works !!! But i obtain a frequency of 555 kHz (while my oled screen has a frequency max of 400 kHz), and the frequency is not equal to 4 MHz / 2 ???
I must be missing something here...
Do you have an idea ?
Thank you :-)
Christophe