Hi
I'm trying to start my first example on MSP430FR5739 using blinking led code . When I debug and run the code this message is displayed and the LED is not
blinking
this is the message :
MSP430: There were 70 (code) and 66 (data) bytes written to FLASH/FRAM. The expected RAM usage is 160 (uninitialized data + stack) bytes.
what this message means and how can I fix it ?
Thanks for help
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P1DIR |= BIT0;
P1OUT |= BIT0;
while(1)
{
P1OUT ^= BIT0;
__delay_cycles(100000);
}
}