We're using MSP-FET430UIF on our manufacturing line to program a MSP430G2553. We're using MSP430Flasher.exe to do the programming.
Programming works fine.
However, after programming we need to power off the target device.
We've tried using the various combinations of the MSP430Flasher.exe -z exit specification command line options to attempt this. These options correctly set the output voltage on pin 2 of the target connector of the MSP-FET430UIF. However, the reset pin (pin 1 of the target connector) continues to be driven high, preventing our target device from fully powering down.
When the MSP-FET430UIF powers down the target, we need it to also drive pin 1 drive low, or go hi-Z.
Is there a way to accomplish this?
Thanks!