Hi All,
I am using a rev 1.1 Red MSP-EXP432P401R launch pad. (I have tried this with the black one as well.)
I am using the 430Boost Sharp96 Boosterpack.
I am using an TI-RTOS 2.16.0.08
I am using MSP432 Driverlib 3.10.00.09
I am trying to get the Sharp 128x128 LCD Display to work. I have been partially successful, let me explain.
In the 430Boost Sharp96 example I can build and run the 96x96 version on the Booster. If I modify the SharpLCD96.h file and set the LCD size to 128 by 128, this example works fine with the 128x128 LCD in the boosterpack. In other words, I can simple switch between the two LCD Displays by changing the extents in the header file. This example is not using RTOS. I think this may be important.
I now have an RTOS application the application uses both I2C and the LCD. It too works perfectly fine with the 96x96. As soon as I try to change to the 128x128 I get nothing. As a matter of fact, if I run the 430Boost example and then run the RTOS, the screen retains the graphic from the 430boost example. It is like it is getting nothing.
You help would be greatly appreciated.
Thanks
John