Hello,
I am working on MSP430F5419A mcu.
I am doing Interfacing between MSP430F5419A and GSM808 module using UART commmication . In this , i am sending SMS to MCU through GSM modem for do some operation based on SMS interrupt and send back ACK of SMS (for confirmation of SMS deliver or not).
Problem : With continuous debug mode, getting ACK of SMS (reply of SMS ) but if i remove debug mode and MCU direct run without emulator interrupt operation doing fine but ACK (reply of SMS ) is not coming.
what is the problem in when code is run without emulator? Is it required any configuration in properties of project?
Is this problem of MCU or GSM module?
Please give me inputs on above problem.
Regards,
Sanjay.