Other Parts Discussed in Thread: MSP430FR5738, MSP430FR5739
Tool/software: Code Composer Studio
I have added a number of Scalar Graphs to the GUI screen I have developed - and data is plotting quite nicely. The issue I am having is that I cannot fix the scale to have a min and max value. I am wanting the graph to show say between 0 and 8, but if the values received always float around 7 to 7.5, then the min and max are also scaled to around those values. Is there a way to pre-define the min and max? On the control, it has series_0_min and series_0_max, but when I populate these values, it does not fix the scale for that control. Could you please advise?
Thanks