Hi. I have a MSP430G2553 that I am using to develop a system to select from one of four options using leds as indicators of which option is currently selectable and a push button to make the selection. The way I have the code configured, it works as expected something close to 80% of the time. My question is can anyone see how I have incorrectly coded this given that the trace on an oscilloscope shows observed button bounce is shorter than software debounce time?
In the code, I use Timer1_A1 in continuous mode to cycle between 4 leds with a delay. I have used a software debounce (from bennthomsen.wordpress.com/engineering-toolbox/ti-msp430-launchpad/using-the-switches/) that uses the watchdog timer set to create a 32ms delay (WDT_MDLY_32) before re enabling the interrupt on the push button pin. The interrupt is set to trigger on a low-to-high transition and the pin is pulled up so that the button triggers the interrupt on release. I have only observed bounce times on the order of < 200 us on this breadboarded circuit so either I didn't set the button up correctly or I have failed to implement the watchdog software delay correctly.
Thanks for any help that you can provide!
Nick
#include <msp430.h> #define LED1 BIT4 #define LED2 BIT5 #define LED3 BIT0 #define LED4 BIT1 #define PB1 BIT2 volatile int timerOverflow = 0; volatile int pushButtonPressed = 0; void turnOffLeds(void); /* * main.c */ int main(void) { int selectingLED = 1; int ledPosit = 0; int myLeds[4] = {LED1, LED2, LED3, LED4}; WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer //set ports as i/o P1SEL = 0; P1SEL2 = 0; P1DIR |= (LED1 + LED2); P1OUT &= ~(LED1 + LED2); //turn these off P2SEL = 0; P2SEL2 = 0; P2DIR |= (LED3 + LED4); P2OUT &= ~(LED3 + LED4); //turn these off //start with this LED ON P1OUT = LED1; //set up pushbutton P2DIR &= ~PB1; // set up as input pin P2REN |= PB1; // enable pull up/down resistor P2OUT |= PB1; // select pull up P2IES &= ~PB1; // enable interrupt to trigger on rising edge P2IFG &= ~PB1; // clear interrupt flag P2IE |= PB1; // enable interrupts on this pin /* * MC_2 continuous up, ID_3 input divide by 8, TASSEL_2 SMCLK, enable interrupt */ TA1CTL = MC_2 + TASSEL_2 + ID_3 + TAIE; __enable_interrupt(); for(;;) { int lpbPressed = pushButtonPressed; if(lpbPressed == 1) { if (selectingLED == 1) { // disable timer interrupt TA1CTL &= ~TAIE; selectingLED = 0; }else{ //enable timer interrupt and back to displaying LEDs TA1CTL |= TAIE; selectingLED = 1; //turnOffLeds(); } pushButtonPressed = 0; //enable push button interrupt P2IE |= PB1; } if(timerOverflow == 1) { timerOverflow = 0; //turn off all leds turnOffLeds(); if (ledPosit < 2) //check for PORT1 { P1OUT |= myLeds[ledPosit]; }else{ // must be PORT2 P2OUT |= myLeds[ledPosit]; } if (ledPosit > 2) { ledPosit = 0; }else{ ledPosit = ledPosit + 1; } } } return 0; } void turnOffLeds(void) { P1OUT &= ~(LED1 + LED2); P2OUT &= ~(LED3 + LED4); } #pragma vector = PORT2_VECTOR __interrupt void PORT2_ISR (void) { P2IFG &= ~PB1; // clear flag P2IE &= ~PB1; // disable interrupt /* WDTCTL = WDT_MDLY_32; // start and set WD timer for btn debounce IFG1 &= ~WDTIFG; // clear flag IE1 |= WDTIE; // enable WDT interrupt */ pushButtonPressed = 1; } #pragma vector = WDT_VECTOR __interrupt void WDT_ISR(void) { IE1 &= ~WDTIE; // disable WDT IFG1 &= ~WDTIFG; // clear flag WDTCTL = WDTPW | WDTHOLD; // stop WD //enable push button interrupt P2IE |= PB1; } #pragma vector = TIMER1_A1_VECTOR __interrupt void Timer1_A1_ISR (void) { static int timerCounter = 0; switch(TA1IV){ case 10://overflow TA1IFG { if (timerCounter == 3) { timerOverflow = 1; timerCounter = 0; }else{ timerCounter = timerCounter + 1; } break; } default: //oops break; } }