Part Number: MSP430-ADC10
Hi! I'd like to sample the onboard voltage references of either 2.5 (REF2_5) or 1.5 volts so that I can measure when my chips VCC gets below a certain threshold.
for example:
I know that If I'm measuring from GND to 3.0 volts and sampling 2.5 volts my ADC10MEM value should be 0x355 or 853. If my vcc drops to 2.8 my ADC10MEM value will be 0x392 or 914.
I don't have to actually convert these values to a voltage readout the only thing that matters is knowing when the Vcc gets below a set threshold.
working with a MSP430-EXP430G2 on CSS