Tool/software: Code Composer Studio
Hello everyone,
I am using USB module of msp430f5529 and the program i am doing is the receive data program using USB module.I executed the code successfully but after that how to check the o/p I don't know? I attached the code below.Please help me with the same.
I have tried serial windows like Teraterm and Hyperterminal but couldn't get the o/p.
/* --COPYRIGHT--,BSD
* Copyright (c) 2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
/*
* ======== main.c ========
* Receive 1K bytes from terminal application:
*
* This example implements a device whose only purpose is to receive a 1K chunk
* of data from the host. It begins by prompting the user to press any key.
* When the user does so, it asks for 1K of data. Any data received after that
* point will count toward the 1K (1024 byte) goal. When 1K has been received,
* the program thanks the user, and the process repeats
*
+----------------------------------------------------------------------------+
* Please refer to the Examples Guide for more details.
* ---------------------------------------------------------------------------*/
#include <string.h>
#include "driverlib.h"
#include "USB_config/descriptors.h"
#include "USB_API/USB_Common/device.h"
#include "USB_API/USB_Common/usb.h"
#include "USB_API/USB_CDC_API/UsbCdc.h"
#include "USB_app/usbConstructs.h"
/*
* NOTE: Modify hal.h to select a specific evaluation board and customize for
* your own board.
*/
#include "hal.h"
// Global flags set by events
volatile uint8_t bCDCDataReceived_event = FALSE;
volatile uint8_t bDataReceiveCompleted_event = FALSE;
// Application globals
uint8_t dataBuff[1024];
char outString[40] = "";
uint16_t x;
char pakOutString[16];
volatile uint16_t usbEvents = USB_VBUSON_EVENTMASK + USB_VBUSOFF_EVENTMASK +
USB_DATARECEIVED_EVENTMASK + USB_USBSUSPEND_EVENTMASK +
USB_USBRESUME_EVENTMASK +
USB_USBRESET_EVENTMASK;
/*
* ======== main ========
*/
void main (void)
{
WDT_A_hold(WDT_A_BASE); // Stop watchdog timer
// Minumum Vcore setting required for the USB API is PMM_CORE_LEVEL_2 .
PMM_setVCore(PMM_CORE_LEVEL_2);
USBHAL_initPorts(); // Config GPIOS for low-power (output low)
USBHAL_initClocks(8000000); // Config clocks. MCLK=SMCLK=FLL=8MHz; ACLK=REFO=32kHz
USB_setup(TRUE, TRUE); // Init USB & events; if a host is present, connect
__enable_interrupt(); // Enable interrupts globally
while (1)
{
// Check the USB state and directly main loop accordingly
switch (USB_getConnectionState())
{
// This case is executed while your device is enumerated on the
// USB host
case ST_ENUM_ACTIVE:
// Enter LPM0 until an event occurs.
__bis_SR_register(LPM0_bits + GIE);
// This flag would have been set by the
// handleDataReceived event; this event is only
// enabled when waiting
// for 'press any key'
if (bCDCDataReceived_event){
bCDCDataReceived_event = FALSE;
// Change the event flags, in preparation for receiving 1K
// data. No more data-received. We only used this for
// 'press any key'
usbEvents &= ~USB_DATARECEIVED_EVENTMASK;
// But enable receive-completed; we want to be prompted when
// 1K data has been received
usbEvents |= USB_RECEIVECOMPLETED_EVENTMASK;
USB_setEnabledEvents(usbEvents);
// We don't care what char the key-press was so we reject it
USBCDC_rejectData(CDC0_INTFNUM);
// Prompt user for 1K data.
strcpy(outString,"I'm ready to receive 1K of data.\r\n");
// Send it over USB. If it failed for some reason; abort and
// leave the main loop
if (USBCDC_sendDataAndWaitTillDone((uint8_t*)outString,
strlen(outString),CDC0_INTFNUM,0)){
USBCDC_abortSend(&x,CDC0_INTFNUM);
break;
}
// Set up rcv operation for 1K data
// If USBCDC_receiveData fails because of surprise removal
// or suspended by host abotr and leave main loop
if (USBCDC_receiveData(dataBuff,1024, CDC0_INTFNUM) ==
USBCDC_BUS_NOT_AVAILABLE){
USBCDC_abortReceive(&x,CDC0_INTFNUM);
break;
}
}
// This flag would have been set by the handleReceiveCompleted
// event; this event is only enabled while receiving 1K data,
// and signals that all 1K has been received
if (bDataReceiveCompleted_event){
bDataReceiveCompleted_event = FALSE;
// Prepare the outgoing string
strcpy(outString,"Thanks for the data.\r\n");
// Send the response over USB. If it failed for some reason
// abort and leave the main loop
if (USBCDC_sendDataInBackground((uint8_t*)outString,
strlen(outString),CDC0_INTFNUM,0)){
USBCDC_abortSend(&x,CDC0_INTFNUM);
break;
}
// Change the event flags, in preparation for 'press any key'
// No more receive-completed.
usbEvents &= ~USB_RECEIVECOMPLETED_EVENTMASK;
// This will tell us that data -- any key -- has arrived
usbEvents |= USB_DATARECEIVED_EVENTMASK;
USB_setEnabledEvents(usbEvents);
}
break;
// These cases are executed while your device is disconnected from
// the host (meaning, not enumerated); enumerated but suspended
// by the host, or connected to a powered hub without a USB host
// present.
case ST_PHYS_DISCONNECTED:
case ST_ENUM_SUSPENDED:
case ST_PHYS_CONNECTED_NOENUM_SUSP:
__bis_SR_register(LPM3_bits + GIE);
_NOP();
break;
// The default is executed for the momentary state
// ST_ENUM_IN_PROGRESS. Usually, this state only last a few
// seconds. Be sure not to enter LPM3 in this state; USB
// communication is taking place here, and therefore the mode must
// be LPM0 or active-CPU.
case ST_ENUM_IN_PROGRESS:
default:;
}
} // while(1)
} // main()
/*
* ======== UNMI_ISR ========
*/
#if defined(__TI_COMPILER_VERSION__) || (__IAR_SYSTEMS_ICC__)
#pragma vector = UNMI_VECTOR
__interrupt void UNMI_ISR (void)
#elif defined(__GNUC__) && (__MSP430__)
void __attribute__ ((interrupt(UNMI_VECTOR))) UNMI_ISR (void)
#else
#error Compiler not found!
#endif
{
switch (__even_in_range(SYSUNIV, SYSUNIV_BUSIFG ))
{
case SYSUNIV_NONE:
__no_operation();
break;
case SYSUNIV_NMIIFG:
__no_operation();
break;
case SYSUNIV_OFIFG:
UCS_clearFaultFlag(UCS_XT2OFFG);
UCS_clearFaultFlag(UCS_DCOFFG);
SFR_clearInterrupt(SFR_OSCILLATOR_FAULT_INTERRUPT);
break;
case SYSUNIV_ACCVIFG:
__no_operation();
break;
case SYSUNIV_BUSIFG:
// If the CPU accesses USB memory while the USB module is
// suspended, a "bus error" can occur. This generates an NMI. If
// USB is automatically disconnecting in your software, set a
// breakpoint here and see if execution hits it. See the
// Programmer's Guide for more information.
SYSBERRIV = 0; // clear bus error flag
USB_disable(); // Disable
}
}
//Released_Version_5_10_00_17