This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: ADS1198: False leadoff detection for negative channels in AD1198 continuesly, Critical issue

Other Parts Discussed in Thread: MSP430F5438A

Dear Brian,

                   Thank you, for your inputs and support to fix this issue.

Please, help me in updating the firmware by using binary file  project_name.out.

currently we are following method to update the firmware.

Tools used: Code composer studio V5

Programmer & Debugger used  : MSP-FET430UIF ( MSP430 USB - debug Interface).

steps are as follows.

  •  set the project configuration to Release - MSP430F5438A EXP[Active] in workspace.
  • Build All ( Projecct --> Build- All).
  • Debug ( Run -- Debug).

    I want to use only binary file project_name.out to update the firmware in all devices. Please clarify following ASAP.

  1. Methods or steps need to be followed to update the firmware using only binary file(project_name.out).
  2. Is there any way to update the firmware OTA( Over the air )?.

Thanks and Regards,

Bhairu

**Attention** This is a public forum