Other Parts Discussed in Thread: MSP-FET, , MSP430FR5969
I have a new board where I was planning on using the BSL to program it, but I can't get it to show any signs of life. When I use the BSL scripter to send a TX_BSL_VERSION command there is no response from the blank 2311. The TXD pin is low, so it looks like the UART isn't getting initialized. I also made sure to run the scripter within 10s of a reset so it doesn't time out.
Here's a list of things I've checked:
- power is good 3.3V
- !RST is high
- TEST is low
- serial output from BSL scripter looks good on the scope 8e1 @ 9600 bps
Is there anything else I'm missing? I have two boards that both act the same way. Can connections of any of the other pins stop the BSL from starting?