Other Parts Discussed in Thread: MSP-FET, MSP430WARE
I want to measure internal temperature sensor value. I used example code that is msp430x09x_apool_adc_06.c (APOOL_ADC, Sampled Temperature and Convert to oC) but it does not work properly. I observed that APINT (A-POOL Integer Conversion Value Register) value is just increasing second by second. I have tried to debug with IAR Embedded Workbench via MSP-FET FLASH EMULATION TOOL and MSP-TS430L092 Target Board. Please help me to sort this kind of problem. I tried to turn on P1.4 pin that is tied LED with temperature sensor value. If the DegC value is between 15 and 30, it will turn on LED otherwise it doesn't work. I saw that my LED turn on after 20 seconds. First it blinked three times and then it permanently turns on until 40 seconds. Finally it turns off dramatically because my APINT value is just increasing. Why does it work? Can someone help me please?
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
/* Description: ADC Temperature Sample */
/****************************A_POOL ADC Conversion *******************************/
/* */
/* */
/* +----L092---+ */
/* |*1 14 | */
/* | 2 13 | */
/* | 3 12 | */
/* | 4 11 | */
/* | 5 10 | */
/* | 6 9 | */
/* | 7 8 | */
/* +-----------+ */
/* */
/* D.Dang/ D.Archbold/ D.Szmulewicz /F. Chen */
/* Texas Instruments Inc. */
/* Built with IAR Version 5.51.1 and CCS Verison 5.3.00090 */
/*********************************************************************************/
#include <msp430.h>
int Result;
volatile short int DegC;
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
// Begin Configuration of the A-POOL registers
APCTL = 0; // Clear APCTL register
APIE |= EOCIE; // Enable Interrupt for End of Conversion
APTRIM = REFTSEL;
APVDIV = TMPSEN; // Enable Temperature Sensor
APCNF = CMPON+DBON+CONVON+APREFON+CLKSEL_MCLK; // Configure A-POOL elements, Select MCLK as A-POOL Clock Source
P1DIR |= BIT0 + BIT1 + BIT4;
while(1)
{
APCTL = OSEL+ODEN+OSWP+APPSEL_4+APNSEL_5; // Set Channels and Start Conversion--+ODEN+
APINT = 0x00; // Clear ADC-DAC-REG
APIFG = 0;
APCTL |= CBSTP+SBSTP+RUNSTOP;
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts enabled
Result = APINT;
DegC =(((Result-179)*125)/58) + 30; // Refer to datasheet for accuracy and offset specs
if(DegC>15&&DegC<30){
P1OUT|=BIT4;
}
else{
P1OUT&=~BIT4;
}
__no_operation(); // SET BREAKPOINT HERE
}
}
//A_POOL Interrupt Service Routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=APOOL_VECTOR
__interrupt void A_POOL(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(APOOL_VECTOR))) A_POOL (void)
#else
#error Compiler not supported!
#endif
{
APIFG = 0; // Clear Interrupt Flag
__bic_SR_register_on_exit(LPM0_bits); // Exit Active to calculate Temperature
}