Hi Champs,
My customer found one piece MSP430G2433's content would be modified in aging test lab, and total volume in the lab is about 75 sets. The temperature is about 50℃, the moisture is about 75%. And the address is located in code sector. For example, '0xB0' is modified to '0xB8', and all the modification is from 0 to 1. After checking with customer, there is no any Flash operating code in their project, and the voltage is stable.
Would you kindly suggest where the problem comes from? And also is there any tests that I can do?
Thanks.
BR,
Young