I am trying to use the LDOONIFG flag and LDOONIE interrupt to indicate when there is adequate power on the LDOI pin.
According to the MSP430 User Manual the LDOONIFG flag can be used to indicate that the supply voltage on LDOI has risen above the launch voltage. In addition ot this flag an interrupt should be generated when LDOONIE is set.
Unfortunately these two signals (along with the LDOOFFFG flag and LDOOFFIE Interrupt enable) do not seem to function without the LDO PWR module being enabled by having LDOEN set to 1.
Is there a way that I can have the LDOONIFG flag be active without turning on the LOW PWR? I would like to detect a change of state for the power without having the extra power consumption of have the LDO PWR turned on.