Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
I would like to use MSP432P401R to read data from 10 sensors.
In outdoor application, there are many waterproof cases and connectors and the distance between sensors and MSP432 is 1 or 2 meters.
So, I don't want the MSP432 to read analog data directly.
This is hard for me to do calibration.
I think the digital communication is the better way.
First, I think I can use 4 hardware UART->RS232 and 6 software I/O->RS232 to read sensor data.
But I don't know is it suitable?
Second, I think I can use RS485 for multiple communication.
But I worry that one of sensor is broken then make the communication suspended.
Has someone know how to do?
Any suggestions will be appreciated.
YHH