Hi,
We will like to understand the architectural advantages / disadvantages for a industrial IOT Platform with MSPXX + CCxxx (For Eg MSP430F6435 + CC2520) Vs Wireless WMCU(CC2650) solution
Power Consumption:
MSP430F6435 + CC2520 Active power supply: 2.1mA(8mhz/Flash) + 1.6mA (Active) = 3.7mA
Wireless MCU CC2650 Active Power Supply: 1.45mA + 0.248mA (at 8Mhz) + RF Core Idle 0.237mA? = 1.9MA
Wireless MCU solution holds advantage.?
Cost:
Wireless MCU solution holds advantage.
Form Factor:
Wireless MCU solution holds advantage.
Flexibility For multiple Radio technologies:
a. MSPxx+ CCxx Solution has flexibility to change radios
b. With Wireless MCU can we have the same flexibility of using external radio(on UART/SPI) if needed by switching off the internal Radio Core? Do we need to use TI RTOS for this or HAL apis are provided open source?
Applications:
a. Are Wireless MCU CC2650 and MSP both equally good for industrial low power applications?
Guidance/inputs/view would help.
Regards,
Prashant