Part Number: MSP432P401R
Hello! I'm using the Fuel Tank MKII Battery BoosterPack Plug-In Module with a MSP-EXP432P401R Rev. 2.1 Launchpad and the example from MSP432 Simplelink SDK 1.40.1.00 (boostxl_batpakmkii_fuelgauge_MSP_EXP432P401R_nortos_ccs).
I've noticed that when first running the example it does not read the State of Charge and Remaining Capacity (it says 0% and 0 mAh). All other parameters are read fine. These are the steps to reproduce the issue:
1. Connect battery to plug-in module;
2. Connect the plug-in module to the Launchpad;
3. Disconnect 3V3 and 5V jumpers from the Launchpad;
4. Connect the USB cable to the Launchpad;
5. Switch the battery pack on.
6. Program and run the example.
When this happens, if I stop the program and restart, then it reads OK.
Can anybody reproduce the issue? Is there a problem with my hardware or is it a software-related problem?