Part Number: MSP432P401R
i use the SWD protocol to operate the MSP432,and i can connect to the MSP432 correctly
but when i want to reset the MCU through JTAG command,it didn't take effect.
i write the command 0x006901 to SYS_REBOOT_CTL register, but the MCU do not reset
and i also try to write 0x006901 to SYS_RESET_REQ register,and it didn't take effect too.
so i want to know is i want to reset the MSP432 through JTAG,which register should i use?