Other Parts Discussed in Thread: ENERGIA, MSP-EXP430F5529LP, MSP-TS430PN80USB, MSP430USBDEVPACK
Hello everybody,
I'm trying to make use of the USB BSL of the MSP430F5529. First i uploaded the blink sketch using Energia through the Spy-bi-wire interface( with success) and then i wanted to upload the same code using the USB BSL so i connected the USB from the PC to VBUS, DM, DP and ground, then i connected the PUR pin to 3.3V through a resistor, i also connected a 4 Mhz cristal to the HF pins. When i tried to upload the sketch, i failed. I couldn't find the reason why i didn't succeed. I also removed the JTAG wires when i uploaded through USB. Did any one tried a setup like that with a successful attempt ? Thanks a lot in advance.