Part Number: MSP432P401R
Hi all,
My MSP432 Launchpad (Black PCB) cannot select the Launchpad EMT (48MHz) on Energia after it the programming firmware updates itself.
I can compile and load the program using the RED Launchpad Board selected on the Board Manager. But the program cannot run even the Blink example.
It appears to be it is freezing and the LED does not blink. The attachment is the error upon selecting the Launchpad MSP432 EMT(48MHz) and not the RED Launchpad.
What I did is to revert all the previous board definitions and try loading the Blink program and no luck to make it work.
When I load the older version of Energia, it reupdates again the firmware program for the programmer and loads the Blink program and it works.
Does anyone have an idea how to use the Black MSP432 Launchpad on the lastest version of Energia or what causes this problem?
Thanks in advanced,
Leo B. Pestañas