This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

MSP430FR2311 and energia

Intellectual 260 points

Replies: 3

Views: 1464

Can we add MSP430FR2311 launchpad board to the Energia IDE. i dont find this board in the boards manager. can anyone help me with this?

  • Energia support for the MSP-EXP430FR2311 is expected in the next version release but is not yet available limited, please see Robert's explanation below.

    Regards,
    Ryan

    To better aid the community, please click on the "This Resolved my issue" button whenever a post answers your question!

  • MSP430FR2311 is available in Energia but is hidden. The reason for this is that the FR2311 has very little memory to work with. With 4K FRAM / 1K SRAM the most you will be able to run is along the lines of Serial + Blinky. 

    You can enable it at your own risk. To set the right expectation, I will not be able to support you if things don't turn out to work / you run out of memory.

    To enable support. Install the latest core through the board manager in Energia.

    Edit the board file boards.txt in the location below and uncomment the MSP430FR2311 section.

    On GNU/Linuxes: ~/.energia15/packages/energia/hardware/msp430/1.0.3
    On Windows: %LOCALAPPDATA%\Energia15\packages\hardware\msp430\1.0.3
    On MacOS: ~/Library/Energia15/packages/hardware/msp430/1.0.3
    Robert

  • In reply to Robert Wessels:

    Thank you so much for the suggestion sir.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.