Other Parts Discussed in Thread: ADS1118, ENERGIA,
Tool/software: Code Composer Studio
Hi , We bought MSP430 and ADS1118 booster pack for a project to acquire temperature data using a k-type thermocouple and print it to serial COM port. We created a data acquisition app in C# that reads serial COM periodically , show it in a windows form and save it as csv file with time stamp . We did it successfully using Arduino and MAX6675 , but we are not able to achieve it using TI assembly :( . We tried both in energia and CCS . We are able to flash MSP using TI's MSP430 flasher downloaded from TI software support . Temperature is successfully printed in ADS1118 LCD ,so we re able to upload simple skeches like hello world and blink. But the temperature acquisition and printing to serial is not working ,
Anybody have the energia or ccs version source code of the default temperature acquisition program which is pre-loaded in MSP430(which is now in bin format and we cant edit) .
The program from the above link is also not working . Please help!!!