I am trying to code my MSP432 in C to make 4 switches control one of your 7-segment LEDs and the other 4 control the other 7-segment display. It is your choice what LED behavior you want. The switch also have to be interrupt driven. Here is what i have so far:
// Basic I2C Driver.
//
#include <stdint.h>
#include "msp.h"
#include "InputOutput.h"
#define NVIC_ISER1 (HWREG32(0xE000E104)) /* Irq 32 to 63 Set Enable Register */
//----------------------------------------
// eUSCI wait until START and address are transmitted
//----------------------------------------
void WaitStart(void)
{
while ((UCB0CTLW0 & UCTXSTT) != 0);
}
//----------------------------------------
// eUSCI wait until STOP is complete
//----------------------------------------
void WaitStop(void)
{
while ((UCB0CTLW0 & UCTXSTP) != 0);
}
//----------------------------------------
// eUSCI wait until TX is complete
//----------------------------------------
void WaitTx(void)
{
while ((UCB0IFG & UCTXIFG0) == 0);
}
//----------------------------------------
// eUSCI wait until RX is complete
//----------------------------------------
void WaitRx(void)
{
while ((UCB0IFG & UCRXIFG0) == 0);
}
//----------------------------------------
// eUSCI generate start
//----------------------------------------
void GenStart(void)
{
UCB0CTLW0 |= UCTXSTT;
}
//----------------------------------------
// eUSCI generate stop
//----------------------------------------
void GenStop(void)
{
UCB0CTLW0 |= UCTXSTP;
}
////////////////////////////////////////////////////////////////////////
//
// Enable interrupts on P4.6. Port4_IRQHandler should get called below whenever
// a one of the 8 inputs to I2C_SWITCH change--provided P4.6 is connected
// to the INT signal on I2C_0.
//
void ConfigureInterrupts()
{
// Make sure P4.6 is an input and allow it to generate interrupts.
// Needs an internal pull-up resistor too.
P4DIR &= ~BIT6;
P4IES |= BIT6;
P4IE |= BIT6;
P4REN |= BIT6;
P4OUT |= BIT6;
P4IFG &= ~BIT6;
NVIC_ISER1 |= BIT6; // IRQ 38
}
// Function prototype
extern void EnableInterrupts(void); // defined in startup_msp432.s as a subroutine
// In Keil, name the ISR exactly the following...
void PORT4_IRQHandler(void)
{
// interrupt generated on any port 4 pin
//
// if ConfigureInterrupts() is called above, maskable interrupts
// are enabled [via the EnableInterrupts() function], and
// the INT pin of I2C_0 is connected to P4.6, this ISR will be called
// whenver a DIP switch changes
//
// this eliminate the need for the MSP432 CPU to poll the switches periodically
// to see if anything has changed
//
// ordinarily, ISRs should be short and defer further processing
// tasks to the main loop--however, at this point the main loop does nothing
// so it is OK to do other processing tasks here
//
// Always clear the port-level latch.
P4IFG &= ~BIT6;
// MSP432 will now resume whatever it was doing when the interrupt
// came in
}
// No parameters
void InitI2C(void)
{
//
// Configure with the following parameters:
// * 7-bit addresses.
// * single master environment.
// * MSP432 is always master.
// * I2C mode.
// * Synchronous mode.
// * SMCLK is source.
// * Automatically trigger address ACK.
// * No interrupts.
//
UCB0CTLW0 |= UCSWRST; // hold USCI in reset.
P1SEL0 |= 0xC0; // P1.7 (SCL) and P1.6 (SDA) multiplexing.
P1SEL1 &= ~0xC0;
UCB0CTLW0 |= (UCMST | UCMODE_3 | UCSYNC | UCSSEL_2);
UCB0BRW = 400; // Divide SMCLK down by this factor to get SCL.
UCB0CTLW0 &= ~UCSWRST; // release USCI reset.
}
//
// Send a byte of data to the I2C target.
// [Note there is no error checking here.]
//
void OutI2C(unsigned char address, unsigned char data)
{
UCB0I2CSA = address; // UCB0I2CSA = <expander addr w/o R/W bit>.
UCB0CTLW0 |= UCTR; // TX.
GenStart(); // Generate a START.
WaitStart(); // Wait for START and slave address to be sent.
WaitTx(); // Wait until it is safe to write to TX buffer.
UCB0TXBUF = data; // UCB0TXBUF = <data> (prep data).
if ((UCB0IFG & UCNACKIFG) == 0) // Check for slave NACK.
{
// I2C slave responded.
WaitTx(); // Wait until data is transferred.
}
else
{
// I2C slave did not respond.
}
GenStop(); // Generate a STOP.
WaitStop(); // Wait for STOP to be sent/ready to go again.
}
//
// Receive a byte of data from the I2C target.
// [Note there is no error checking here.]
//
unsigned char InI2C(unsigned char address)
{
unsigned char retVal;
UCB0I2CSA = address; // UCB0I2CSA = <expander addr w/o R/W bit>.
UCB0CTLW0 &= ~UCTR; // RX.
GenStart(); // Generate a START.
WaitStart(); // Wait for START and slave address to be sent.
if ((UCB0IFG & UCNACKIFG) == 0) // Check for slave NACK.
{
// I2C slave responded. Get data.
WaitRx(); // Wait for data.
retVal = UCB0RXBUF; // Read UCB0RXBUF for data.
}
else
{
// I2C slave did not respond.
}
GenStop(); // Generate a STOP.
WaitStop(); // Wait for STOP to be sent/ready to go again.
return retVal;
}
int main(void)
{
const unsigned char sevSegTable[16] =
{
0x40, // 0
0x79, // 1
0x24, // 2
0x30, // 3
0x19, // 4
0x12, // 5
0x02, // 6
0x78, // 7
0x00, // 8
0x18, // 9
0x08, // A
0x03, // B
0x46, // C
0x21, // D
0x06, // E
0x0E // F
};
// Ex: address = I2C_8574 | I2C_0
// Ex: address = I2C_8574_A | I2C_3
unsigned char switchAddress = I2C_8574 | I2C_0;
unsigned char sevenSegLedAddress = I2C_8574 | I2C_3;
unsigned char sevenSegLedAddress2 = I2C_8574 | I2C_4;
unsigned char data;
ConfigureInterrupts();
EnableInterrupts();
InitI2C();
while (1)
{
data = InI2C(switchAddress);
data = sevSegTable[data & 0xF];
OutI2C(sevenSegLedAddress, data);
}
// this will never be hit (compiler will probably warn)
//return 0;
}
I just don't know how I can shift the switch address to only change one LED and the other 4 change the other. I also made a look up table so that the LED will display a hex number/letter based on the four switches.