Part Number: MSP432P401R
I have spent 3+ months developing software running on an MSP430FR5994 Launchpad... without using MSP430 DriverLib. Now I want to convert that S/W to the MSP432P401R Launchpad and add new features like floating point, output to graphic displays, etc. that are possible with the new, faster H/W.
I believe that there is a tool that helps the conversion and I will start researching it shortly. But I don't just want to convert my S/W, I also want to add to it. I need something like SLAC710c, but focusing on MSP432 instead of MSP430. I need a bunch of standalone examples... no SDK stuff, no DriverLib stuff, no RTOS stuff, no MSP432 ROM stuff... just standalone C code examples... I haven't found them yet. I want code that I enter into CCS with my very own fingers. Code that I understand completely.