Other Parts Discussed in Thread: CODECOMPOSER
Tool/software: Code Composer Studio
I am newbee c programmer so be patient. I have a MSP430 C project in Code Composer Studio 7.3 using windows 7. My project (USB) was working fine and then I tried to add more code to incorporate a SPI interface and everything went sideways. I restored my original code but now have problems that weren't there before. Seems to compile but has several unresolved symbols errors in the linker (I think). I have searched/researched many answers to these types of problems on the forum and tried many things (over the past two days!!) and cannot resolve my problem. Possibly I made things worse by copying library/functions directly into my project directory but still didn't seem to change anything. The errors are related to standard MSP430 functions, not my code. My project tree looks like:
Errors from Console are:
From everything I have read it indicates that either I have a compiler library path problem or a linker file path problem. Tried a lot of combinations to no avail. Following are the compiler and linker path info:
f I look in my repository of library stuff downloaded from TI you can see that the dma.h and dma.c files which reference the error message lines in the files are there and I don't understand why the linker can't do its thing.
In the linker under library files I noticed the original libmath.a file didn't point to anything so I found one and added it (not help). Also the libc.a points to a section of 3 directories (different versions of a tool) which each have a different version of libc.a and I think I tried all of them. See below for directories
I have tried every combination of all the linker/compiler path/file combinations with no improvement. What am I doing wrong??