I started the OOTB demo from scratch with the new procedure mentioned at Thu, Apr 12 2018 3:07 PM.
I built the OOTB code with CCS Cloud and uploaded it to the MSP432E LaunchPad.
No luck, I'm stuck with the following error:
This command is supported only during initialization.
as per
pid xxxxxxxxxxxxxxxx xxxxxxxxxxxxxxxx.m2.exosite.io/ Welcome to the MSP-EXP432E401Y LaunchPad's, Out of box Demo. MAC Address: xxxxxxxxxxxxxxxx PIK found in EEPROM XXXXXXXXXXXX Connected to Exosite server. No Token found in EEPROM. > pid xxxxxxxxxxxxxxxx This command is supported only during initialization. CloudTask: Bad response, ecode: -1 during : 2 action. Resetting connection. Connected to Exosite server. No Token found in EEPROM. CloudError: Server returned : 502 during : 1 action. Retrying >
How to enter initialisation mode to specify the PID again?
Thank you and best regards,