Other Parts Discussed in Thread: TMS3705, TMS37157,
Hello,
I'd like to calculate the CRC-16 acc. to CCITT to communicate via TMS3705 to TMS37157.
I have a working code just using shift operation.
I adopted this: https://en.wikipedia.org/wiki/Computation_of_cyclic_redundancy_checks, code fragment 5, shift register based division, LSB first and it works perfect.
The MSP430F6659 has a hardware CRC module and I'd like to use this, because it is the faster and more elegant solution.
This is the code I tested so far, but it didn't deliver the correct result in comparison to the software solution:
unsigned int i, CRC_Result, CRC_Init = 0x3791; CRCRESR = CRC_Init; // CRCINIRES = CRC_Init; for(i=0; i<length; i++) { CRCDIRB = string[i]; } CRC_Result = CRCRESR; return(CRC_Result);
I try to use the reverse (see above) and the non reverse registers, but non of the version seem to work.
Please help
Kind regards
Gerd