Tool/software: Code Composer Studio
hi this is harikrishna...
i have doubt like this ..we have driverlib in that __delay_cycles(); function is there..so i am doing on GSM project in that my MSP UART0 is connected to GSM module they are in communicating with each other by AT commands ..and in MSP program RTC is running and for every SECOND interrupt in RTC it is blinking one LED for 100ms delay so..i am having problem like this when AT command is sending from MSP and modem is giving responce perfectly but in MSP UART0 is not taking that responce ...i don't no why it is happening but i felt because of __delay_cycles(); function RTC will disturbing that MSP and GSM modem communication....
is it true or false?
please give a suggestion to avoid that problem
NOTE :some times only it is happening not for all AT commands...