Tool/software: Code Composer Studio
Hi all,
I have already asked this question, but since I did not get a response, I thought I would ask it again for clarity.
I am trying to use the MSP430FR5994 RTC_C module. I have breakpoints for the RTCIV_RTCTEVIFG and the RTCIV_RTCAIFG interrupts. But only the first interrupt is being called. I am attaching my code to help with any questions about setup you may have. For the most part, my setup is similar to the example TI code. Thank you for your help!
/* * mainTest.c * * Created on: Jul 31, 2018 * Author: Sanskriti Joshi */ #include <msp430fr5994.h> int PollingInterval = 2; volatile int counter = 0; int main(void){ MCU_Init(); MCU_Init_Clock(); RTCsetup(); while(1){ __bis_SR_register(GIE|LPM3_bits); } } void MCU_Init() { // configure MCU Pins WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer PM5CTL0 &= ~LOCKLPM5; //disable the GPIO power-on default high-impedance } void MCU_Init_Clock() { PJSEL0 = BIT4 | BIT5; //initialize the LFXT pins CSCTL0_H = CSKEY >> 8; // Unlock CS registers CSCTL0 = CSKEY; CSCTL1 = DCOFSEL_0; // Set DCO = 1MHz (measured with Oscilloscope to be slightly less that 1 MHz) CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK; // set ACLK=VLO;SMCLK=DCO Note: the VLO is typically 10 kHz (measured with Oscilloscope to be slightly less that 10 MHz) CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // set all dividers //start of code added for RTC CSCTL4 &= ~LFXTOFF; //enable the crystal do{ CSCTL5 &= ~LFXTOFFG; //clear LFXT fault flag SFRIFG1 &= ~OFIFG; }while (SFRIFG1 & OFIFG); //test oscillator fault flag //end of code added for real time clock CSCTL0_H = 0; // Lock CS Registers } void RTCsetup(void){ //RTC_C setup RTCCTL0_H = RTCKEY_H; // unlock RTC registers RTCCTL0_L = RTCTEVIE_L | RTCRDYIE_L; //Enable RTC Ready Interrupt and Time Event Interrupt RTCCTL13 = RTCBCD | RTCMODE | RTCHOLD; // Enable BCD mode, enable RTC in calendar mode, hold while date/time values are set //SET date time info RTCYEAR = 0x2018; RTCMON = 0x7; RTCDAY = 0x25; RTCDOW = 0x4; RTCHOUR = 0x12; RTCMIN = 0x50; RTCSEC = 0x00; //RTC clock alarm setup RTCalarmSet(PollingInterval); RTCAMIN |= RTCAE; //enable minute alarm RTCCTL13 &= ~(RTCHOLD); //start RTC RTCCTL0_H = 0; } void RTCalarmSet(int PollingInterval){ RTCAMIN = 0x00; RTCAHOUR = 0x00; RTCADOW = 0x00; RTCADAY =0x00; unsigned int Temp_time = 0; Temp_time = (((RTCMIN >> 4) & 0x0F) * 10) + (RTCMIN & 0x0F); Temp_time += PollingInterval; if(Temp_time > 59){ Temp_time -= 60; RTCAMIN = (Temp_time / 10) << 4; RTCAMIN |= (Temp_time % 10); }else{ RTCAMIN = (Temp_time / 10) << 4; RTCAMIN |= (Temp_time % 10); } } #pragma vector = RTC_C_VECTOR __interrupt void RTC_C_ISR(void){ switch(__even_in_range(RTCIV, RTCIV__RT1PSIFG)){ case RTCIV_RTCTEVIFG: //minuteInterrupt counter = counter - 1; break; case RTCIV_RTCRDYIFG: //secondInterrupt break; case RTCIV_RTCAIFG: //alarm interrupt //RTCalarmSet(PollingInterval); RTCAMIN |= RTCAE; //enable minute alarm counter = counter + 1; break; default: break; } __bic_SR_register_on_exit(LPM3_bits); }