Using ports 1, 3, or 4 for I/O and counter/timer.
Using port 3, can I set and use 6 individual I/O pins to read or write individual bits. Some will be connected to individual external hall effect switches which will have to generate an interrupt for that specific bit input. Can I also use 1-2 TAx Out pins for the counter/timer simultaneously on the same port? Switch input interrupts are more important than TAx out for this port.
Using port 4, same question, but need to use TB0 for very precise PWM output. TB0 output is more important than I/O port out only, no bit input interrupts.