Tool/software: TI-RTOS
Hi,
I have successfully gotten my CPU into LPM4. I exit LPM4 by using one of the hardware buttons on my system to generate an interrupt. I have verified that the ISR is being executed using my debugger. The last statement executed before returning from the interrupt is __bic_SR_register_on_exit( 0xF0 );
The problem arises after returning from the interrupt. My .cfg has timer0 ( instantiated with XGCONF ) associated with a function called heartBeatFxn(). This has period of 25mS, and it is never being executed after RETI. At this point the SR has a value of 0x040C. Also I have verified that TA0 is running.
Is there something I need to do to get the RTOS operating after exiting LPM4 ?
Thank you
Roy