Tool/software: Code Composer Studio
I'm using the MSP430FRBoot example bootloader as a starting point for OTA firmware upgrade for my project. I've been able to build the example projects and step through the firmware upgrade process as described in the MSP430FRBoot app note (SLAA721B). Now I'm trying to use the debugger while running either App1 or App2 prior to updating the linker and address space for my application. However, I can't debug either App1 or App2 with Code Composer Studio. I think what happens is the debugger erases all flash (including the previously loaded MSP430FRBoot) and when I start code execution it jumps to the start of where the MSP430FRBoot used to be.
If I have a project setup for the application space for MSP430FRBoot, what special things do I need to do so I can debug the application with Code Composer Studio? I'm assuming there may need to be some different Run/Debug settings, but I haven't found the right combination yet. Is there anything else I need to change also?