I've been fighting a very strange problem with the USI module. Occasionally, USICNT spontaneously takes on strange values. I've attached a short program that demonstrates the problem. It shows up on different chips (both 14-DIP and TSSOP-14) in various circuit setups, including a simple ez430-F2013. It is extremely timing-sensitive, to the point where slight changes to bus capacitance make the problem show up or disappear.
Am I doing something wrong that's causing this? If not, is there anything I can do to avoid it? It's wreaking havoc with my system.
Thanks!
John-Paul Gignac
;*********************************************************************** ;* This program demonstrates a glitch in the MSP430F2013's USI module. * ;* I've tested it successfully with the EZ430-F2013, as well as other * ;* setups. If the glitch doesn't show up within a few moments, try * ;* modifying the impedance of SCL very slightly by placing your hand * ;* near, or attaching a long (eg, 24 inches) conductor to pin 8. * ;*********************************************************************** #include "msp430x20x2.h" RSEG CSTACK ; Define stack segment RSEG CODE ; Assemble to Flash memory EVEN RESET mov #0x5A80, &0x0120 ; Stop watchdog timer mov.w #SFE(CSTACK),SP ; Initialize the stack pointer ; Set the clock speed to around 1MHz mov #0x86BA, &0x0056 ; Setup pin assignments mov.b #0xFF, &0x0021 ; P1OUT = 0xFF mov.b #0xFF, &0x0022 ; P1DIR = 0xFF mov.b #0x00, &0x0026 ; P1SEL = 0x00 mov.b #0xC0, &0x0027 ; P1REN = 0xC0 ; P1.6 & P1.7 Pullups ; Setup the USI in master mode mov.b #0xCB, &0x0078 ; USICTL0 ; Initiate software reset mov.b #0x50, &0x0079 ; USICTL1 mov.b #0x6A, &0x007A ; USICKCTL ; SMCLK / 8 mov.b #0x00, &0x007B ; USICNT = USIIFGCC mov.b #0xCA, &0x0078 ; Finish the software reset mov.b #0x50, &0x0079 ; Clear the interrupt flags eint main_loop ; Begin with a short delay mov #500, r12 delay dec r12 jne delay clr r7 mov.b #0x08, &0x007B ; Start transmitting 8 bits ;**************************************************************** ;* We watch for the glitch while the byte is being transmitted. * ;* The symptom is that USICNT spontaneously takes on a value * ;* higher than what was assigned to it. A typical observed * ;* value is around 0x1A. * ;**************************************************************** watch_for_glitch cmp.b #0x09, &0x007B jhs glitch tst r7 jeq watch_for_glitch jmp main_loop glitch ;************************************************************************ ;* Place a breakpoint here or trigger your oscilloscope on P1.0 (pin 2) * ;************************************************************************ dint bic.b #1, &0x0021 bis.b #1, &0x0021 mov.b #0x00, &0x007B bic.b #3, &0x0079 eint jmp main_loop ;***************************** ;* Interrupt Service Routine * ;***************************** USI_ISR mov #1, r7 bic.b #1, &0x0079 reti COMMON INTVEC ORG RESET_VECTOR ; MSP430 RESET Vector DW RESET ; ORG USI_VECTOR ; USICNT DW USI_ISR ; END