I am using Energia 1.8.7E20, downloaded from here: http://www.energia.nu/download/. I have the EXP-MSP430FR5739 board connected. I am unable to upload the example blink sketch to the board. I get the following error message:
------------------------
Sketch uses 972 bytes (6%) of program storage space. Maximum is 15743 bytes.
Global variables use 20 bytes (1%) of dynamic memory, leaving 1004 bytes for local variables. Maximum is 1024 bytes.
java.io.IOException: Cannot run program "{runtime.tools.mspdebug.path}/mspdebug": CreateProcess error=2, The system cannot find the file specified
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:26)
at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:129)
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:207)
at cc.arduino.UploaderUtils.upload(UploaderUtils.java:82)
at processing.app.SketchController.upload(SketchController.java:736)
at processing.app.SketchController.exportApplet(SketchController.java:703)
at processing.app.Editor$DefaultExportHandler.run(Editor.java:2028)
at java.lang.Thread.run(Thread.java:748)
Caused by: java.io.IOException: CreateProcess error=2, The system cannot find the file specified
at java.lang.ProcessImpl.create(Native Method)
at java.lang.ProcessImpl.<init>(ProcessImpl.java:386)
at java.lang.ProcessImpl.start(ProcessImpl.java:137)
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
... 8 more
An error occurred while uploading the sketch
------------------------
Any idea how to resolve this?
I am running Windows 7. The previous version of Energia, 1.6.10E18 works fine (it is still installed on my PC).
Regards,
David