Other Parts Discussed in Thread: MSP-FET, MSP-TS430PM64
Tool/software: Code Composer Studio
hi
thank you sir,
I m using msp430F135 . while debugging code using MSP-FET430UIF (4 wire JTAG) following error pop up
MSP430: Can't Single Step Target Program: Could not single step device
some time i get this error
MSP430: Trouble Halting Target CPU: Internal error
No source available for "0x0"
i m using code simply blinking led .
#include <msp430.h> int main(void) { WDTCTL = WDT_MDLY_32; // Set Watchdog Timer interval to ~30ms IE1 |= WDTIE; // Enable WDT interrupt P1DIR |= 0x01; // Set P1.0 to output direction _BIS_SR(LPM0_bits + GIE); // Enter LPM0 w/ interrupt } // Watchdog Timer interrupt service routine #pragma vector=WDT_VECTOR __interrupt void watchdog_timer(void) { P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR }
so pls help me out this problem.