Part Number: MSP432P401R
I would like to use the MSP432P401R "Flash Information Memory" to store code trace data.
Section 6.4.1.2 of the MSP432P401R Data Sheet (document number SLAS826G-MARCH 2015-Revised September 2017) implies there are two 4kB sectors up for grabs, but it's a procedure to write to them- so what is that procedure?
I'm guessing I would put 16 bytes into a buffer (called what or located where?), then pulse the required number of times as indicated in the "Flash Information Descriptor" (reference sectipns 4.9.3.3 the MSP432Pxx Technical Reference Manual, document number SLAU356H-MARCH 2015- Revised December 2017). Is that the general idea?
Or perhaps someone can point me to an API that does this.