Other Parts Discussed in Thread: MSP430I2040
Support,
Is it possible and can you recommend how to hook up multiple MSP430i20xx's so the sampling is synchronized across all the devices?
Regards,
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Support,
Is it possible and can you recommend how to hook up multiple MSP430i20xx's so the sampling is synchronized across all the devices?
Regards,
Marc
Tom,
It really comes down to comparing an MSP430F6775x solution to what can be done with the i20xx.
The technical requirements is to have SD24 sampling clock sync'd across multiple devices. Today, the 6775x uses the TACLK input on each device supplied from a high precision clock distribution device. It is not dependent on the device's main clock. This guarantees common SD24 clock independent of any DCO jitter.
The i20xx does not have TACLK as an option to supply the SD24 sample clock
I think the answer is pretty clear at this point. It cannot be done. There seems to be no way to guarantee a common SD24 clock across multiple devices.
Regards,
Marc
Jace,
I think i'm following. Here is what I'm thinking ... ultimately, as before, my goal is to get SD24s fired as close to the same time. Do you think this would work?
* Setup GPIO as interrupt (I want this to be HIGH Priority)
* ISR will 'kick' SD24 by register write
* SD24 will sample (how long does this take? ~4 clocks?)
* ISR will 'turn off' SD24 by register write
* ISR will clear the interrupt flash and wait ...
**Attention** This is a public forum