Other Parts Discussed in Thread: ENERGYTRACE
Hi,
I have loaded the out-of-box example for the MSP-EXP430FR5994 board. Then I ran the example code with the energy trace active. After the board started and the statement '__bis_SR_register(LPM3_bits | GIE);' got executed, the energy trace showed power consumption settling at approximately 1.5 mWatt (see attached image). Now, as per my understanding, 1.5 mWatt is corresponding to 455 micro ampere (at 3.3 volts). So, my question is that this doesn't comply with the datasheet claim of 700 nano ampere power consumption in LPM3 mode (datasheet article no. 6.4 Operating Modes). Am I missing something somewhere?
Using the launchpad in debug mode, I verified that the statement '__bis_SR_register(LPM3_bits | GIE);' is getting executed. Also, during the test, the jumpers RXD & TXD were removed, SBWTDIO & SBWTCK were inserted. Super capacitor jumpers were not populated. J7 was populated on board.
-
Thank You
-
Regards
Soumyajit