Hi,
It says in the MSP430F5438A Experimenter Board User guide that the LCD used on the board is 138 x 110 Hitachi HD66753. When I checked the code given in UserExperience example, it is using the SPI protocol for the LCD interface. So I googled and found datasheets for HD66753.
- I was unable to find one which supports 138 x 110 resolution.
- All the data-sheets showed an I2C interface as opposed to an SPI.
Can someone at TI help me in getting the correct LCD data-sheet? I wanted to understand the lcd interface for which the HAL's were written and provided.
Thanks in advance