Hello,
I am using the msp430fr5994, and I need help setting up the eCOMP. I am a student at North Carolina State University, and I have never used the eCOMP before. The project I am working on involves charging and discharging a makeshift 29 pF capacitor and measuring the time it takes to reach a certain voltage range. I am charging the capacitor up to 3.3 volts, then setting the pin direction low to allow it to discharge. I am trying to measure the time it takes to go from the start of the discharge to the voltage range between 1 and 1.1 volts. I have looked over the eCOMP registers in the user guide and there are quite a few I don't understand. Does anyone have an easy way to set up the eCOMP to check between 1 and 1.1 volts?
Thank you.