Tool/software: Code Composer Studio
I tryed to build an example project: EVM430-F6779_CT_3V_3C_50Hz . Every went OK without any error and it created the CCS and IAR projects.
I want to build the project using CCS and the TI compiler, importing the project in CCS should satisfy this condition but when starts to link this is the error output:
warning #10207-D: automatic RTS selection: resolving index library "libc.a" to "rts430x_lc_ld_eabi.lib", but "rts430x_lc_ld_eabi.lib" was not found
error #10234-D: unresolved symbols remain
warning #10202-D: no suitable entry-point found; setting to 0
error #10010: errors encountered during linking; "EVM430-F6779_CT_3V_3C_50Hz.out" not built
>> Compilation failure
makefile:228: recipe for target 'EVM430-F6779_CT_3V_3C_50Hz.out' failed
gmake[1]: *** [EVM430-F6779_CT_3V_3C_50Hz.out] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
gmake: *** [all] Error 2
makefile:224: recipe for target 'all' failed
I am using CCS Studio Version: 7.2.0.
OS Windows 7 Professional