Other Parts Discussed in Thread: CAPTIVATE-PHONE, CAPTIVATE-FR2633
Tool/software: Code Composer Studio
Hi.
My customers made the MSP430FR2633 custom board and mutual capacitance sensor sheet.
As with the evaluation boards CAPTIVATE-FR2633 and CAPTIVATE-PHONE, they are connected using connectors.
And they want to detect that the connector has been disconnected.
For example (on the evaluation board), we would like to detect that the connection between CAPTIVATE-FR2633 and CAPTIVATE-PHONE has been disconnected.
Question:
Are there any parameters that can check the connection status?
If this is not the case, prepare GND pin on the sensor sheet and consider the method of detecting from GPIO (pullup) of FR2633.
Regards,
Rei