I installed CCS 4.2.1.00004 yesterday on Windows XP SP3, to program an EM-CC430F6137-900 with an MSP-FET430UIF. This is a pristine install on a pristine machine.
The installation program created a device under "Ports (COM & LPT)" called "MSP-FET430UIF - VCP (COM3)".
In the IDE, my target configuration connection choices are:
Data Snapshot Viewer
TI MSP430 LPT1
TI MSP430 LPT2
TI MSP430 LPT3
TI MSP430 USB1
TI MSP430 USB2
TI MSP430 USB3
Note that COM3 is not available as a selection, nor is any other COM port.
When I attempt to debug the blink application, I get the following error:
Error initializing emulator:
No USB FET was found
I expect that I have overlooked something simple, and that there is a way to use a COM port, but in a day of searching I have been unable to resolve this.
How do I tell CCS to use COM3 (or any COM port) as the target connection?
Thanks for your help.